Beli flexible coupler di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- Sung-IL Machinery Oldham Type Flexible CouplingDeskripsi:SOH Series Classification- SOH series transmits motion through the middle spacer and is particularly excellent for absorption of parallel misalignment.- It has a simple structure for easier self-maintenance.- It enables reaction force on the shaft to be reduced by moving the spacer even though there is parallel misalignment.- Sung-il Machinery provides various spacer types which are allowed to be used in special circumstances.- If the shaft has to be inserted deeper than L1 value, we can provide appropriate center-through sleeves.- Center-Through (TH) is standard for the following models, SOH-6,8,10,12, SOHM-12C, SOH-70C, 90C, 120C and all sizes of SOHMP & SOHV series.- The standard color of spacer for SOH-6, 8, 10, 12 is white, but the material is the identical Polyacetal(POM).atribut:
- Angular (°): 1.5
- End-play (mm): 0.15
- Fastening Method: General Clamp Type
- Item Type: SOH-SERIES
- Sung-IL Machinery Radial Beam Type Flexible CouplingDeskripsi:- SRB series is one-piece metal coupling with no backlash and absorbs misalignment through its slit structures.- SRB series is made of ultra high strength aluminum alloy material (AL-7075-T6) in order to enhance its durability.INNER-RELIEF AREASRB series has the “relief” space structure in the middle area, in case there is interference that causes damages.ROUND-SHAPED SLITSSRB series has rounded slits(cuts) structure to disperse stress concentration.atribut:
- Angular (°): 2.5
- Item Type: SRB-SERIES
- DAYTON Jaw CouplingDeskripsi:General purpose straight jaw coupling hubs attach to motor and equipment shafts using a set screw or keyway. Two couplings of the same size are locked together with a compatible straight jaw spider. These hubs are interchangeable with other brands according to the coupling size identifier.atribut:
- UNSPSC: 31163003
- System of Measurement: Inch
- Orientalmotor Coupling Flexible (Kopler)Deskripsi:Flexible Coupling (5 mm to 8 mm)Please contact your local sales office for proper sizing or more information.
- Sung-IL Machinery Jaw Type Flexible CouplingDeskripsi:- Power transmission through the spider (sleeve) in the middle- The highest durability comparing to other coupling series- Various clamping methods available- High precision with preloaded assembly- A Sleeve (Spider) is the medium that transmits motion absorbing impact and misalignment and it is the core part of Jaw couplings.- Hytrel®(made by Dupont) is superior in terms of mechanical strength, abrasion resistance and heat resistance whereas TPU (Thermoplastic polyurethane) has higher damping capacity.- According to material and shore stiffness, there are 3 types of sleeves, RD(Hytrel, Sh 63D), GR(Hytrel, Sh 98A) and BL(TPU, Sh 98A) respectively.atribut:
- Angular (°): 1
- End-play (mm): -0.4 to +1.0
- Sung-IL Machinery Oldham Type Flexible CouplingDeskripsi:SOH Series Classification. - SOH series transmits motion through the middle spacer and is particularly excellent for absorption of parallel misalignment. - It has a simple structure for easier self-maintenance. - It enables reaction force on the shaft to be reduced by moving the spacer even though there is parallel misalignment. - Sung-il Machinery provides various spacer types which are allowed to be used in special circumstances. - If the shaft has to be inserted deeper than L1 value, we can provide appropriate center-through sleeves. - Please indicate additional mark (TH) next to the part no. Please refer to “HOW TO ORDER” for more details. - Center-Through (TH) is standard for the following models, SOH-6,8,10,12, SOHM-12C, SOH-70C, 90C, 120C and all sizes of SOHMP & SOHV series. - The standard color of spacer for SOH-6, 8, 10, 12 is white, but the material is the identical Polyacetal (POM).
- Mitsuboshi Hyperflex Coupling Mt Type Elastic Body (Kopling)Deskripsi:Oil, excellent wear resistance, elasticity of polyurethane is also available as a standard.
- INDOMAKERS Coupling Flexible Aluminium (Kopler)atribut:
- Length (mm): 25
- Outer Diameter (mm): 19
- Material: Aluminium
- FCL Spare Part (Karet Coupling)atribut:
- Type: Rubber
- TB WOOD S Jaw CouplingDeskripsi:General purpose straight jaw coupling hubs attach to motor and equipment shafts using a set screw or keyway. Two couplings of the same size are locked together with a compatible straight jaw spider. These hubs are interchangeable with other brands according to the coupling size identifier.atribut:
- Sub Brand: L-Jaw
- Sung-IL Machinery Double Disk Type Flexible CouplingDeskripsi:- The recommended shaft tolerance is h7.- Custom process (e.g. non-standard Inner diameter, special tolerance etc.) is also available upon a special request in prior to order placement.- Keyway is available. (Optional)- Due to interference of the middle parts, make sure the shaft is only inserted into L1 depth for IDs with ★ mark.- Side-clamp Hub Split is available (Optional)Slip Torque- The below table shows the actual permissible torque values when the slip torque value is lower than the coupling’s max. torque value.- If the slip torque value is lower than the coupling’s max. torque value, please check and compare between the slip torque in the below table and the operating torque value of the connected motor. It is safer to size up the coupling or use a key/keyway when the slip torque value is lower than the motor’s operating torque.- The below slip torque values may be subject to change according to different testing conditions. (e.g. shaft tolerance, Surface roughness, or acceleration/deceleration of driving shafts). On the other hand, the values could be affected when a different kind of fastening screw is used (body material or surface treatment). Therefore, we recommend you test under the same conditions before mounting.atribut:
- Dimension L (mm): 52.6
- Dimension L1 (mm): 19
- Dimension F (mm): 6.3
- Fastening Torque (N m): 8
- Static Torsional Stiffness (N m/rad): 7000
- Angular (°): 1.5
- Parallel (mm): 0.2
- Fastening Method: General clamp type
- Shape: Cylinder
- End Play (mm): ± 0.5
- Inside Diameter d1 (mm): 22
- Inside Diameter d2 (mm): 22
- Maximum Speed (rpm): 7500
- Maximum Torque (N m): 44
- Moment of Inertia (kg.m²): 1.1x10-4
- Outside Diameter D (mm): 54
- Rated Torque (N m): 22
- Screw Size: M5
- Standard Inner Diameter (d1, d2) (mm): 22x22
- Sung-IL Machinery Urethane Flexible CouplingDeskripsi:- SFC series is flexible with Urethane material and is especially excellent for absorbing misalignment to a greater extent. - The middle Urethane structure absorbs external impacts and absorbs vibration.
- Sung-IL Machinery Flexible CouplingDeskripsi:- The Moment of Inertia and Mass values are based on products with max. Inner diameter. - Max. torque/rated torque is the value regarding to a coupling's self-durability and is not related to slip-torque between the coupling bore and the shaft.atribut:
- Fastening Method: General clamp type
- Shape: Cylinder
Daftar Harga flexible coupler Terbaru October 2026
| Sung-IL Machinery Oldham Type Flexible Coupling | Rp279.900 |
| Sung-IL Machinery Radial Beam Type Flexible Coupling | Rp249.900 |
| Sung-IL Machinery Jaw Coupling | Rp249.900 |
| DAYTON Jaw Coupling | Rp429.900 |
| Orientalmotor Coupling Flexible (Kopler) | Rp889.900 |
| Sung-IL Machinery Jaw Type Flexible Coupling | Rp249.900 |
| Sung-IL Machinery Oldham Type Flexible Coupling | Rp229.900 |
| Mitsuboshi Hyperflex Coupling Mt Type Elastic Body (Kopling) | Rp289.900 |
| Sung-IL Machinery Cross Joint Coupling | Rp469.900 |
| INDOMAKERS Coupling Flexible Aluminium (Kopler) | Rp20.900 |
Data diperbarui pada 09/10/2026 (Harga belum termasuk PPN)























































































































































/k2P107599722-1.jpg)


/P102373101-1.jpg)

/meP107884806-1.jpg)
/2fP104857087-2.jpg)
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
/WD-40%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/OLFA%20Cutter%20Knife%20Safety%20(Pisau%20Cutter)%20149B%201pc/S009054721-2.jpg)
/Joyko%20Gel%20Ink%20Pen%20Q%20(Pulpen%20G2%20%2F%20Pulpen%20Gel)%20GP-265%20Black%200_5mm%201box(12pcs)/qmS009904958-2.jpg)
/REXCO%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20RX-SP0009%20500ml%2F415g%201pc/2bS000076083-4.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Tahan%20Minyak/Sarung%20Tangan%20Tahan%20Minyak%20Karet%20Nitril/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)%2037-176%20Size%209%201pair/S000074366-1.jpg)

%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)/IKA%20(Copy%20Paper)%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20IKF%20PC%2070%20A4G%201ream/8pS035166313-2.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Kesehatan/Pertolongan%20Pertama%2C%20Kebutuhan%20Higienis/Perban%2C%20Kain%20Kasa/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)%201box(100pcs)/h6S039287618-2.jpg)
/3M%20Post-it%20654%20Sticky%20Notes%20(Kertas%20Memo)%20654-5CY%201pack(5pads)/5iS030245198-4.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)

/monotaro_id%20Cable%20Ties%204_8x250mm%20(Pengikat%20%2F%20Kabel%20Tis)%20White%201pack(100pcs)/2xS039549105-2.jpg)
/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)